Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65982, , TPS65987, TPS65988
Hi Team,
We are working on custom design for HDMI to type-c alt.[i.e., hdmi over type-c]
Our hardware team has interacted with TI support team and finalised to use
TUSB546EVM comprising TPS65982 as PD controller with TUSB546 crossover switch. But we will replace TPS65982 by TPS65987D in our custom design,
We are planning to implement this design in snapdragon 820 based carrier board running with debian OS with linux kernel version 4.14.96.
We would like to ask few questions on that :
1) Do we need a linux kernel driver for TPS65982(PD controller) or the firmware flashed inside the TPS65982 will do the required functionality?
2) Is the firmware already loaded or should we flash the firmware to the TPS65982?
3) If firmware has to be flashed, Is there a procedure to flash the firmware in the linux environment?
4) Does the TUSB546 mux require any linux kernel driver or is it just a switch which does not require any linux kernel driver ?
Regards,
deepika.s