Part Number: DS25BR440
Hi there,
please have review on the tested input signal level.
questions is:
1. input signal VH may lower than 100mV, input VL may higher than -100mV. however, according the datasheet, the maximum value of VH is 100mV, the maximum VL is -100mV.
the output signal eye is large enough. in this case, is there any potential risk for the input signal level?
test condition: 25 ℃, 2.37Gbps.
BRs,
Shubiao