Part Number: DS90UB953-Q1
Hello,
You wrote that there are ready design proposals for up to 1 amp. Could you please provide me with these.
(See: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/994072/ds90ub953-q1-poc-filter-verification-for-ser-des-fpd-link-3-camera)
We are currently verifying our design and getting in some cases CRC errors in the back-channel, when the current flow becomes too large. The MAP Tests seems to me very good.
Our goal is a connection with up to 750 mA at a line length between approx. 1 m and 15 m.
At the Moment we only work with a 10 µH Choke and 3 x Ferrits at the DS90UB953, but it seems to me that the ferrits that available to me are not fit and an alternative solution is needed.
Regards,
Dirk