Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP, USB2ANY
Hi team,
My customer design with our 953 and 954 FPD-link device, but face to I2C no ACK during Soc communication with 954.
I have search on E2E post( as below link), and get feedback from customer.
Please find customer's feedback below in red. Could you help to solve this issue? thanks.
- What's your I2C pull-ups?
Pull-ups is 1kohm.
- What is the I2C address of the 954?
IDX pin Rup is 78.7kohm and Rdown is 97.6k, so the I2C address is 0x7A.
- The I2C address can be shown in 7-bit or 8-bit mode. Make sure you are using the right I2C address.
Two kinds of address have been tested. 0x7A and 0x3D, and still no ack appears in communication between soc and 954.
- Can you read reg 0x00 from the 954 and see what it gives back?
Because there is no ack signal, so the reg value can't be read.
Below is the figure of SDA and SCL.

As you can see, the ack position where the SDA should be pull low is high. Could you help analyze the reason here?
The clk is 25MHz.
Thanks and looking forward to your reply.
Best regards,
Jasper