Part Number: TPS25750
Hello,
We have set the max charge current to 0.5A (see attached config file). Once a phone is connected it charges with 1A @5V.
Do you see anything in the config that could cause this?
Thank you and best regards,
Ambroise
{"questionnaire":{"version":"7.0.2.1","answers":[8,null,null,0,2,1,1,null,0,"1216",null,null,null,null,null],"options":{},"configID":"1216","vendorID":"0000"},"configuration":{"data":{"selected_ace":[{"register":6,"data":[0,0,0,0,0,0,0,0]},{"register":22,"data":[10,48,48,77,0,0,0,0,0,0,3]},{"register":50,"data":[1,168,42,50,144,1,38,50,144,1,0,44,177,4,0,44,65,6,0,0,0,0,0,0,0,0,0,0,0,0,0]},{"register":51,"data":[1,50,144,1,0,44,209,2,0,44,177,4,0,44,65,6,0,69,65,6,0,0,0,0,0,0,0,0,0]},{"register":92,"data":[143,12,0,0,0,0,0,0,0,16,0,0,0,0,0,0,48,0,0,0,0,0,0,0,0,12,0,0,0,0,0,0,0,0,0,0,0,73,11,12,0,0,43,3,0,0,29,35,33]}]}}}