Part Number: TCAN1051HV
Other Parts Discussed in Thread: TCAN1051, SN65HVD230, ISO1044
Hi.
Currently we are using CAN transceiver SN65HVD230 with success, and we want to substitute it by a TCAN1051 on the next PCB layout because it is 'fault-protected' and withstands more voltage on the bus lines H and L, we would select a part number which supports +-70V.
I have a doubt about TCAN1051, exactly regarding the pin 'S' that selects Normal Mode or Silent Mode. As we don't have any free GPIO pin on the microcontroller that is an ESP32-WROOM module, we can't control 'S' pin through it, and I would connect 'S' pin directly to GND, in order to set the Normal Mode constantly on the TCAN1051. My doubt is, if I do this, will the TCAN1051 be driving the bus constantly in a manner it will interfere in the communications of the remaining devices on the bus?
And also, I would like to ask if there is some transceiver from TI that withstand +-70V on the bus pins, and that are pin-to-pin compatible with SN65HVD230? That works exactly or very similar as SN65HVD230 but that is fault-protected? +-70V?
Regards,
Jeferson.