Part Number: TCA9545A
Other Parts Discussed in Thread: TCA4311A
Hi
We are using the TCA9545A in the following configuration (see image below), with the TCA9545A and master I2C controller powered from VCC_1, and a device on an output port powered from VCC_2 (and pulled-up to VCC_2). We have a special case where we need to program the device before VCC_1 is present, which means the TCA9545A is not powered on but there will be I2C transactions happening on it's output pins.
When VCC_1 on the TCA9545A is not present (or below UVLO threshold), are the I2C output ports high-impedance, or could there be some conduction path that would cause issues with this approach?
We are trying to understand if we need an I2C isolator (e.g. TCA4311A or similar) to separate the I2C buses when the TCA9545A is not powered.

Thanks