Part Number: LMH1297
Hello expert,
I have question regarding configured value of LMH1297's VOD and DEM by register.
I had confirmed about the configurable setting by register regarding VOD and DEM on this thread.
In this thread, I confirmed that VOD and DEM can be configured as following parameter's
VOD="000", "010", "100", "110"
DEM= "000", "010", "111"
But I cannot found any description regarding the correspondence between register setting and configured value as like as follows.
Would you tell me it?
Thank you and best regards,
Kazuki Kuramochi