Other Parts Discussed in Thread: TIDA-050012, TIDA-050014
Hi,
I am currently in the process of developing a product which will incorporate a USB-C / USB Power Delivery Source and am using the TPS65987D as the Type-C/Power Delivery controller. The design uses the TIDA-050012 Source Board reference design as a general guide for implementation. I also have the USB-C-PD-DUO-EVM as a reference and to use as a USB-C PD sink to test our product.
The issue I am having is when the source/sink negotiate 5V voltage level, it is not possible to place more than ~1.2A load on the sink output before some sort of protection mode kicks in, disconnecting the USB_VBUS. After this happens, PD negotiation restarts, and the sink powers back up. I explored the documentation and settings in the TPS6598x Application Customization Tool, and changed a few things that seemed like they might matter (undervoltage trip point, etc) with no effect. The other voltages (9V, 15V, 20V) operate to our full current requirement (3A) without issue. The power supply used in our design can deliver 0-3.5A at 5V and all the other voltage settings. A DC electronic load is being used as the load for the sink.
When I do this same test using the Evaluation Source and Sink board, with the default configuration loaded from the Application Customization Tool, the behavior is exactly the same (restart at 5V/~1.2A, works ok on other voltage settings). I tried a few different manufacturer's USB-C cables between source and sink but there was no change.
Do you know why I can't reach the full 5V/3A, even with the eval module? Apologies in advance if I am missing an obvious answer for this in the documentation or on this forum.
-Collin