Part Number: TPS65994AD
Other Parts Discussed in Thread: TPS65994,
Hi expert,
I have two qustions on the TPS65994
1. The datasheet says the following:“A portion of the digital core contains ROM memory which contains all the necessary firmware required to execute Type-C and PD applications. In addition, a section of the ROM, called boot code, is capable of initializing the TPS65994AD, loading of device configuration information and loading any code patches into volatile memory in the digital core.”
How are patches loaded into the boot code?
2. Table 8-4 in the spec shows that the EC I2C is used to load the patch and app config. Is the I2C_EC port the only way to do this?. Can the TBT controller also be used to load the patch and app config?

Thanks