Part Number: DP83822HF
Hi,
I want to connect RGMII MODE, did not understand how I connect it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Evgeny,
Please refer to section 8.4.1.3 of the datasheet for information on RGMII mode. Figure 8-7 describes how to connect the DP83822HF to the MAC.
Thanks,
David
I want PHY to run in the RGMII interface, according to the Datasheet I conected like this:
Is it okay ?

Hi Evgeny,
Yes, this is correct. Ensure pin 28 is configured with mode 2 or 3 bootstrapping to enable RGMII mode. Also ensure pin 26 is placed in mode 1 to set the 25Mhz reference clock.
Thanks,
David