Part Number: LMH1218
LMH1218 fail to output 12G-SDI 4K Video:
BARCO and SONY medical displays are tested with both displays failed to display SDI video.
BARCO display prompted "no signal", and SONY display prompted "unknown".
In some rare occasions, SONY display prompted "3840x2160", which is the correct video resolution, and flashed out the distorted video image frame, then went back to "unknown" repeatedly. But after some SW reloading, SONY display went back to "unknown".
SW and HW design:
4K video source is GT transceiver of Xilinx Zynq ZU4, which is transmitting 11.88Gbps 12G-SDI video frames.
Video Format: 3840x2160 60FPS YUV422 10bit pixel.
According to GT status registers, the video transmitting is synchronized to 4K video standard timing, some like active size, sync width, front porch, back porch and so on.
At the same time, LMH1218 is working OK, CDR stays locked to 11.88Gbps SMPTE.