This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: Requirements for crystal

Part Number: DP83826E

Hi team,


DP83826 datasheet for this device lists the equivalent series resistance of the crystal used as 50Ω MAX. The spec of the crystal customer are considering adopting is 60Ω max, which appears not to be an fit.
The crystal manufacturer has commented that there is no problem as an oscillation stability condition as long as the negative resistance is at least 5 times the equivalent series resistance value for matching.

Is there any concern to use it?

Best regards,

Hideki