Part Number: MLVD20XEVM
Hi, I am trying to use this evaluation board for the first time. I can't get an output on any of the boards I have using a Keysight U2761A function generator.
What I am trying to do at this point is to get an output from the LVD205 Via J6 by jumpering W1 through W4 to VCC, I have VCC and VCC 01 jumpered together, as well as both grounds. As far as I can tell, it should enable the transmit and disable the receive. Pin 4 of the 205 has been verified as high, as is the power to the chip.
At this point the input at J2 is a square wave, 3MHz, +2V/-1V voltage levels. VCC = 3.3VDC.
The outputs at P2 are 0.5VDC and 1.3VDC, respectively.
I even tried tying the input to VCC and then GND to see if the output would change states but that did not show any change in output state either.
The boards draw 32mA when idle, seems normal to me.
Any idea what I might be missing here? Seems the operation should be pretty straightforward. I think I have tried everything. Why is the transmit not enabling?
Thanks.