Part Number: TIOL1115EVM
Other Parts Discussed in Thread: TIOL1113, TIOL111, TIOL1115
Hello,
I have a TIOL1115EVM board, which i'm trying to connect to an Arduino using UART.
GROUND, TX, and RX are connected to the Arduino pins. Ground on ground, TX on TX and RX on RX. A master is connected to the TIOL board.
My problem is that the TX voltage is 1.8V. It's impossible to send something from the arduino to the TIOL board.
Plus, i can't power the Arduino with the VCC In/out pin without having the LED NFAULT blinking. Is it normal ?
I can't find anything about uart communication in datasheet. I've tried to disconnect EN, to put 10K resistance pull-up, nothing works.
Thanks for your help !