Part Number: DS90UB933-Q1
Dear team,
Could you please help clarify below drive strength register? It means larger output amplitude? Or larger output current? When do I need to set this bit to 1?

Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB933-Q1
Dear team,
Could you please help clarify below drive strength register? It means larger output amplitude? Or larger output current? When do I need to set this bit to 1?

Thanks & Best Regards,
Sherry
Hello Sherry,
SER reg0x01[6] RDS bit only configures the drive strength of GPO pins (pins 15-18) when set as outputs. This bit has nothing to do with the forward channel signal strength!
Hi Jaradat,
Thanks for your reply!
Could you please tell me what is the high drive strength and low drive strength?
Thanks & Best Regards,
Sherry
Hello Sherry,
Any reason why you are looking for these details?
I do not have specific numbers now, but if this is very important for you, I can discuss this internally with the team!