Dear Team,
About TUSB4041I-Q1
The TEST pin (17pin) is pulled down with 4.7kΩ, but the potential of 17pin is about 1.2V.
8pin, 9pin, 10pin are also pulled down, but they do not fall to the ground.
What could be the cause?
We are in trouble because the IC doesn't work.
Oscillation does not start either.
Thenks