Part Number: TUSB522PEVM
Other Parts Discussed in Thread: TUSB522P
We did an experiment today:
200mV differential signal was added to pins 8 and 9 (attempts were made in the frequency range of 1m ~ 20m). The signal was measured on pins 23 and 22, and no differential signal was obtained.
Similarly, it is useless to do the same experiment with 20, 19pin and 11, 12Pin.
Measured, the power supply is normal, EN_ RXD is high.
As above, please help confirm the reason?