Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: CDCE913-Q1
Hi Expert,
Our customer use 941 +948 in their project. Previously 941 uses DSI clock as input clock and it displays well. Then they use external clock as REFCLK which is generated by CDCE913-q1. The display shakes. They only change bit0-1 from 00 to 01 in register 0x56. Is there any more register they need to change correspondingly?
For 941, they configurate:
- reg 0x17-->0xde;
- reg 0xc6-->0x21;
- reg 0x11-->0x10;
- reg 0x56-->0x1;
- reg 0x1-->0x0;
Thanks a lot for help!
BR,
Elec Cheng