This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988: Application Customization Tool Run from Command Line

Part Number: TPS65988

Hello TI Support,

I'm wondering if it is possible to run the TPS65988 Application Customization tool from the command line?  I would like to be able to open a project and generate the binary without using the GUI for a CI/CD pipeline.  Is that possible?

Also, I can see that it's possible to save the project settings as a JSON file (Project -> Export Settings as JSON).  I don't see how you can load that JSON file as a project.  Is that not possible?

Best regards,

Cory