Part Number: MAX3221
I was working an issue on one of our PCA's to determine why the RS-232 interface was not working. As I troubleshot, I was thinking it was just a bad chip. So, I replaced the chip. It still did not function correctly. I decided to look at the datasheet to see if I was missing a connection or a component.
As I reviewed the datasheet, I noticed that our design uses 0.1uf capacitors on the voltage doubler pins (positive and negative) and on the 5.5V and -5.5v supply generated by the charge pump. The VCC to the chip is 5.0vdc.
When I looked at page 13 of the datasheet, this seems to be an issue. C1 should be a 0.047uf cap and C2 to C4 should be a 0.33uf cap for that condition.
My issue is that it seems like the circuit has been in that condition since its invention and has been operating that way for several years.
So, what are the effects of running the device in a 3.3vdc configuration in a +5vdc environment? What would be the effects? I assume I should be concerned.