If a TUSB217-Q1 detects it has an I2C bus connected will the part still set the registers based on resistors connected to the RX_SEN and BOOST pins.
The datasheet seems to imply that the RX_SEN and BOOST pins would be ignored if an I2C bus is detected, but doesn't explicitly say this.
If, in I2C mode, the RX_SEN and BOOST pins are ignored, is there a default setting for the registers prior to being programmed over I2C, or are the values random?
Is the I2C mode detection simply that the input pins are pulled up, or does it require some activity?
Kind regards
Andrew