This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3223E: Searching TI solution

Part Number: TRS3223E
Other Parts Discussed in Thread: TRS3232E-Q1, TRS3232E, TRSF3232E

Hi team

There is a good new that we could DIN TI product!

Customer is looking for the RS232 Driver (need automotic part )

This is a AVM system project.

1. Please help suggest TI solution, THX

2.TRS3232E-Q1 is a good solution?

TRS3232E-Q1.pdf

  • Hi Kygo,

    TRS3232E-Q1 contains two RS-232 line drivers and two RS-232 line receivers. It supports higher ESD protection with +-15-kV IEC ESD protection. The device operates up to 250kbit/s, but is p2p compatible with TRSF3232E, which is the high-speed device (1 Mbit/s). This device is offered in the PW package type. If you upgrade to the "F" version, you have choices of PW (TSSOP) and RGT/VQFN (square) package types. 

    Did you mean to attach the datasheet of TRS3232E-Q1? I don't have much information about customer application to define a RS-232 device for them. Does the customer want to share schematic, electrical specification requirements, etc?

    Regards,

    Tyler