Part Number: TCA6424A
Other Parts Discussed in Thread: TCA6507
hi team,
Cam TCA6424A used to driver LED and adjust LED brightness?
Jiawei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jiawei,
Yes, it can be used to drive LEDs, but please ensure you keep within the recommended operating conditions of the device. Each pin is recommended to sink no more than 25 mA. The total continuous current through GND should not exceed 200 mA.
Regarding brightness, I would look at the TCA6507, which is specifically designed to drive and adjust the brightness of LEDs.
Best,
Danny