Part Number: TDP142EVM
Other Parts Discussed in Thread: TDP142
Hello, I am currently experiencing an issue with the TDP142EVM when used between a Dell WD19TB Dock and a monitor. The host (DisplayPort source) device (either a Windows PC or Mac) is able to read the EDID of the monitor and detect the screen, but no image is visible and the screens soon goes to sleep after saying that no DisplayPort signal is being detected, any ideas why this might be the case?
List of Jumper states:
J1: Low
J2: Low
J3: Open
J4: Low
J5: Low
J6: High
J7: High
J11: Open
J12 : DPPWR
J14: Closed
We originally saw the issue on our product but then moved to the evaluation board to isoalte the failure. Our displayport logs suggest link training is failing.
Thanks,
James