Part Number: DS90UB941AS-Q1
Hi team,
For 941 pairing with 940, can the PWM signal transfer through GPIO on forward channel? The PWM is 20Khz, and the requirement of delay won't more than 0.1%.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Hi team,
For 941 pairing with 940, can the PWM signal transfer through GPIO on forward channel? The PWM is 20Khz, and the requirement of delay won't more than 0.1%.
Thanks!
Hi Jiawei,
GPIO pins can be used to send a PWM signal from the SER to the DES. The maximum frequency of the PWM signal is defined in the AC Electrical Characteristics table in the UB941AS datasheet:

Depending on the PCLK in your system and the single/dual configuration, then the allowable PWM frequency can be determined.
Best,
Justin Phan