Part Number: DP83867IRPAP-EVM
Dear Sir,
We are making use of DP83867IRPAP EVM board.Ethernet phy IC is getting detected and 1Gbps,100Mbps,10Mbps linkup is working fine.But IP is not getting assigned and sometimes junk
IP is getting assigned .
*Is there any Length matching criteria to be considered for RGMII Signals from Processor (i.MX8 QM) to Ethernet PHY?,if yes please let us know the minimum trace length recomemded.
*Please find our boot log prints below,we are getting RX error and CRC errors as shown below.
root@iWave-G27M:~# ethtool -S eth1
NIC statistics:
tx_dropped: 0
tx_packets: 48
tx_broadcast: 17
tx_multicast: 31
tx_crc_errors: 0
tx_undersize: 0
tx_oversize: 0
tx_fragment: 0
tx_jabber: 0
tx_collision: 0
tx_64byte: 7
tx_65to127byte: 16
tx_128to255byte: 10
tx_256to511byte: 9
tx_512to1023byte: 6
tx_1024to2047byte: 0
tx_GTE2048byte: 0
tx_octets: 10268
IEEE_tx_drop: 0
IEEE_tx_frame_ok: 48
IEEE_tx_1col: 0
IEEE_tx_mcol: 0
IEEE_tx_def: 0
IEEE_tx_lcol: 0
IEEE_tx_excol: 0
IEEE_tx_macerr: 0
IEEE_tx_cserr: 0
IEEE_tx_sqe: 0
IEEE_tx_fdxfc: 0
IEEE_tx_octets_ok: 10268
rx_packets: 2349
rx_broadcast: 0
rx_multicast: 0
rx_crc_errors: 2200
rx_undersize: 0
rx_oversize: 0
rx_fragment: 149
rx_jabber: 0
rx_64byte: 1077
rx_65to127byte: 380
rx_128to255byte: 616
rx_256to511byte: 61
rx_512to1023byte: 52
rx_1024to2047byte: 14
rx_GTE2048byte: 0
rx_octets: 315352
IEEE_rx_drop: 0
IEEE_rx_frame_ok: 0
IEEE_rx_crc: 2200
IEEE_rx_align: 0
IEEE_rx_macerr: 0
IEEE_rx_fdxfc: 0
IEEE_rx_octets_ok: 0
Kindly help us with this error,Hoping for your reply.
With Regards,
Yashash