Part Number: TPS65994AE
Other Parts Discussed in Thread: TPS65994, TUSB1044
I have several questions about the TPS65994AE. The design that I am working on has a single port, what do I do with the pins for the second port? Currently I am floating them, but should I be tying these to ground instead?
The second question I have is about the dead-battery startup condition. This design has no internal battery, but instead can be powered from the USB-C port or another power source (such as a barrel jack). If power is applied to the VIN_3V3 pin before PA_VBUS, am I correct in assuming that this does not trigger a dead battery condition? Just want to make sure.
Lastly, can I get a link to the TPS65994 Configuration Tool? This is mentioned in the EVM user guide but I cannot seem to find a link anywhere to download the tool.