Part Number: TCA6416A
Other Parts Discussed in Thread: TCA6416
Hello guys,
One of my customers is using TCA6416APWR for their current mass production.
But they want to use TCA6416PWR instead of TCA6416APWR due to long lead time.
They found that TCA6416 /RESET pin description is different from TCA6416A as the follow.
TCA6416A /RESET pin description:
"Active-low reset input. Connect to VCCI or VCCP through a pull-up resistor, if no active connection is used."
TCA6416 /RESET pin description:
"Active-low reset input. Connect to VCCP through a pullup resistor, if no active connection is used."
At this moment, they have the following questions. Could you please give me your reply for them?
Q1. Is the RESET pin internal circuit different from TCA6416A one?
Q2. In case of TCA6416, can RESET pin be pulled up to VCCI by a resistor if no active connection is used?]
Your reply would much appreciated.
Best regards,
Kazuya.