Part Number: SN65LV1023A
Other Parts Discussed in Thread: SN65LV1224B, , TRS3232
Hi,
Good Day. Customer is working with SN65LV1023A and SN65LV1224B. Please see below his query for your reference. Thank you very much.
I need help selecting an IC for converting multiple RS232 signals and passing it through to an SFP, I understand I can use the TRS3232 for converting 232 into LVTTL by supplying it with 3.3V, but I need help selecting the proper serializer / deserializer IC.
I am concerned that the RS232 signals will not be fast enough for the Serializer IC to confirm there's good data?
I was looking at one like SN65LV1023ADB and SN65LV1224B for deser.
I essentially just want to convert 4 - 8 RS232 signals into an SFP+ so if there's another solution I'd be open to that.
Best Regards,
Ray Vincent