This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO2001: Power-Up and Power-Down of 1.5V/3.3V/PCIR - Part2

Part Number: XIO2001


This is a related question to this post:
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/727336/xio2001-power-up-sequence-pcir 

It looks like following the EVM design will result in PCIR coming down about the same time as the 3.3V rail.
The User Guide for the EVM (p10) was referenced to show how PCIR could be implemented.

It uses an RC Filter from VDD_33 to PCIR, so PCIR comes up just slightly after 3.3V rails.
But that means during power-down, PCIR comes down slightly after the 3.3V rail.

Yet in the PowerDown sequence, it recommends, and Malik corroborated in the above E2E post, PCIR should be removed first...

During power-down, removing PCIR before 1.5V/3.3V is required to ensure that I/O cells of XIO2001 PCI bus are "OFF" then main power can be ramped down.

This contradicts the EVM setup...Could I get some clarification?
Should following the EVM setup, with PCIR connected to 3.3V rail using the RC filter be fine?

PCIR comes up slightly after 3.3V rail, and powers down slightly after 3.3V goes down...
this affect is minimized by selecting the proper RC time constant relative to the 3.3V rail's ramp rate...

Regards,
Darren