Other Parts Discussed in Thread: TUSB9260, TUSB9261
We have a bit of a snafu with regard to a new design using the TUSB9260.
When we went into layout a few months ago, we had the PC footprint made using a the TUSB9260 data manual "Revised July 2010", which had two packages listed in the package options: TUSB9260PAP and TUSB9260PVP. However, only one package drawing was attached: the TUSB9260PAP package. Our layout people dutifully used that drawing. Now when it came time to make the BOM, the only part available appears to be the PVP package, and now the datasheet on the TI website (still with "Revised July 2010" on its cover) only lists the PVP package and shows *its* drawing instead. So now we have boards with footprints that are 20% too large for the parts we have.
What became of the PAP part? (it was listed as "Preview" status in the older datasheet) Are there still plans to produce it? were any made?