Part Number: DP83TD510E
Hello,
I designed a PCB with the DP83TD510E APL PHY and DP83822 ETH PHY configured in repeater mode just like the DP83TD510E-EVM. While doing the indirect discharge to a horizontal plane ESD test, the APL link sometimes breaks then recovers (this is a failure of the ESD test).
I put the DP83TD510E-EVM to the same test. I found it behaves the same way when the ETH PHY is configured as the RMII Master (the APL link sometimes breaks then recovers). However, if I configure the APL PHY as the RMII Master the DP83TD510E-EVM APL link is always fine and passes the indirect ESD discharge to plane test.
My PCB is configured with the ETH PHY as the RMII Master. This was recommended by TI because of risk that the DP83822 will not start up properly if the DP83TD510E is not providing the 50MHz reference clock when the DP83822 starts up.
Can you help me figure out how to ensure reliable startup and passing ESD testing? The product does not have a microcontroller, so I can't configure the PHYs via register writes. I have to use the straps.
Thanks for your help,
Cyrus