Part Number: XIO2001
Dear Sirs,
Is there a way to know if internal reset is active in XIO2001? Can I read GRST# pin to know if internal reset is happening?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XIO2001
Dear Sirs,
Is there a way to know if internal reset is active in XIO2001? Can I read GRST# pin to know if internal reset is happening?
Thank you
Hello Vitor,
No, there is no internal status that can be read for the GRSTz pin because it resets all the registers to their defaults.
When GRST is asserted low, all control registers, state machines, sticky register bits, and power management state machines are initialized to their default state. In addition, the bridge asserts PCI bus reset ( PRST). When the rising edge of GRST occurs, the bridge samples the state of all static control inputs and latches the information internally. If an external serial EEPROM is detected, then a download cycle is initiated. Also, the process to configure and initialize the PCI Express link is started. The bridge starts link training within 80 ms after GRST is deasserted.
Regards,
JMMN