This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: code examples for interfacing with bq25792

Part Number: TPS25750

Do we have host controller code examples available when the TPS25750 is paired up with bq25792? I am particularly interested in controlling the charge enable process (EN_CHG in register REG0F_Charger_Control_0 of the bq25792). 

In this application my customer is struggling with a situation in which the battery is not present and the bq25792 is tripping on OVP. We want to disable the charging before it happens. I understand that manipulating the CE_n pin is the best approach, but hardware limitations prevents them from doing it right away. We want to try to control it via software and a code example would help with the interpretation of TPS25750 host interface TRM. 

Thank you!