Part Number: TUSB9261
Other Parts Discussed in Thread: TIDA-00882
Hi TI,
I am developing a USB 2.0 - SATA adapter with the TUSB9261.
Please, I have the following questions:
1-) What voltage should be on pin 50 (USB_VBUS) (see attached design)?
2-) For a 2.5 inch hard disk is 12V power supply necessary on the SATA connector (see attached design)?
3-) The resistors R5 and R6 with 10 ohm, 1%, 100 mW, 0603 is ok (see attached design)?
4-) Please could you check the attached schematic to evaluate if there is any error? All suggestions are welcome.
Sincerely, thank you very much.
Best Regards