Part Number: TIC12400-Q1
Hi,
Tic12400-q1 inx external circuit: 10nf cap +1k resistor+10nf cap ,
wetting current set to 0.
comparator threshold level set to 4V.
measurement inx pin voltage close to 1V.
but comparator output is high.!!!!, what reason for that?
if input voltage form 0 to 5V (inx pin), then <4V, comparator output is low, >4V comparator output is high.
best regards,
jeff wang