This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI recommendation

Hello:

Please recommend suitable TI chip for the following material requirements:

1、EDP extension IC: supporting edp1 3. The maximum speed is 5.4G; The ESD level of the chip should be 4K

2、Mipi extension IC:supporting Mipi DSI signal extension, can support the maximum rate of 750MHz; The ESD level of the chip should be 4K