Part Number: TPS25750
Other Parts Discussed in Thread: BQ25792
Hi Team,
I would like to use TPS25750 at sink only.
Therefore, I would like to know the behavior of TPS25750 and VBUS when an unusual source device is connected(3 cases).
------
[Q1]
Source device is not compliant USB PD.
I guess that negotiating continues, VBUS repeats 5V and 0V.
Is my understanding correct?
------
[Q2]
Source device is before USB PD Revision 2.0 version1.1.
So, it is a different version from TPS25750(USB PD 3.0).
<For example>
-Sink request of TPS25750 is 15W (Set with GUI)
-Maximum source capability of source device is 10W(5V/2A)
I guess that TPS25750 can complete negotiation so VBUS is 5V/2A.
So, TPS25750 can communicate even if the versions are different.
Is my understanding correct?
------
[Q3]
Source device is 20V/2A setting.
If request sink power of TPS25750 is “45W(15V)” by GUI, will VBUS be 20V?
(I'm worried that VBUS will be limited to 15V.)
If no, is there a setting method that can handle 20V with the sink request 20W?
------
Regards,
Hide