Part Number: TPS25750
Other Parts Discussed in Thread: TPS2121

Hello,
Explanation of design
Scenario 1) I am designing a board where I want to have data communication between the Samsung A7 Lite tab and my MCU over USB as well as power the MCU using power from the Tablet.
Scenario 2) When the A7 lite Adaptive charger will be plugged into my board then my design should charge the A7 lite Tablet as well as power the MCU.
I am working on the design (Please check attached image). As per the guidance from Adam, I have been using the TPS25750 for my design, whereas I have some questions regarding the design.
FYI, I am using ATMEGA32U2 as MCU, it have in built USB peripheral but unfortunately it does not have I2C peripheral.
As per my information Samsung A7 lit tablet has USB Type-C 2.0 and supports fast charging 15W.
Please find my questions below.
1) I believe that I shall need to provide the I2C connector for externally configuring the TPS25750 into the DRP Role.
2) Once Configured in DRP role, do I still need to have the EEPROM connected to TPS25750? in which scenario do I need to have EEPROM Connected.
3) The Samsung adaptive charger is a 5VDC 1.5A charger. The Samsung website says Adaptive charger are QI compatible, dose this means that the VBUS voltage of charger will go above 5V?
4) Is it true that the PP5 pin is a unidirectional pin and we can use it to charge the Tablet up to 5V 3A? If yes then will it be safe to connect Charger VBUS pin to PP5 pin?
5) As my power requirement for the MCU + Motor is not more than 800mA. Also I do not want to go for higher voltage PPHV during powering MCU in absense of charger Hence is there a provision in Application Customization tool where I can restrict PPHV signal to 5V only.
Also I have made the schematic which I would like to share in private for your review and guidance.
Thank you.
Piyush Saxena