Part Number: TCA5405
Hello,
Currently I am testing the TCA5405 using the TCA7408-5405 EVM. I have modified the EVM so circuit other than the TCA5405 is not populated.
I was testing the IC response to reverse current from GPO pin to VCC pin of TCA5405 , when VCC is off (VCC pin has 10k PD).
The test setup is shown below.

The result from the test is shown below.

The result does not match what I expected for few reasons.
1. The current through the resistor does not match up. The current through resistor A and B matches up, but current through the 10K PD on VCC does not match, meaning there is some other current paths.
2. The voltage at node C is lower than expected. Taking the case where resistor A is 1k and resistor B is 0 ohm, I expected the majority of voltage to appear on node C but it didn't.
Based on the result above, I suspect there is another conduction path other than the GPO to VCC diode.
When I conducted a diode test, I see the following values.
- GPO -> VCC : 0.570V
- GND -> GPO : 0.514V
- GPO -> GND : 1.013V
The first two diode value makes sense due to either the protection diode or MOSFET body diode.
I also see a forward diode conduction from GPO to GND for all GPO pins. This seems odd to me and I want clarification on what this is / request for the internal GPO structure to verify.
Sincerely,
Tsugumi