Other Parts Discussed in Thread: CDCLVC1104, TLK1501
Hi,
I have a board that I made that contains four TLK1501s whose GTX_CLK inputs are driven by a CDCLVC1104 clock buffer. The buffer is driven by a Virtex 6 output signal that is located on an eval board that comes up thru a FPGA Mezzanine connector. The clock is single ended and is 40 MHZ.
The TLKs are each hooked up to their own SFP modules. If I connect a short fiber jumper from the TX port to the RX port of channel A, the link works properly and data is passed on to the RX side perfectly. If I do the same for Channel B it works as well. But if I connect the TX of port A to the RX of port B or vice versa, the links do not work and the RX_ER control lines toggle. Could this problem be due to jitter on the GTX_CLK ? or something else which I am missing? What's the difference if the TX signal is originating from the same channel as the RX or from a channel next to it?
Thanks,
Brian