Hi,
I only can find ESD rating specification in "6.2 ESD Ratings",
Does there have any information for ESD air and contact rating?
thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I only can find ESD rating specification in "6.2 ESD Ratings",
Does there have any information for ESD air and contact rating?
thanks!
Jeff
Hi Parker,
So this part doesn't support IEC 61000-4-2 specification, right?
Thanks!
Hi Jeff,
It is not spec'd - so theoretically there would be some protection - we just don't have the data to say what level it is as we didn't run tests against IEC 61000-4-2.
There is ESD protection on the device but the standards that this device were tested to are:
ANSI/ESDA/JEDEC JS-001 (HBM): +/-15kV Bus/Ground Pins | All Pins +/-4kV
Charged-device model (CDM), per JEDEC specification JESD22-C101: +/-1kV
Electrical Fast Transient/Burst, A, B, and GND per IEC 61000-4-4: +/-4kV
Please let me know if you have any other questions!
Best,
Parker Dodson