Hi,
We are using the DS90UB954TRGZTQ1 and DS90UB953 for serializing and Deserializing MIPI data from a High-speed camera. To send the data to the computer we are using the CYUSB3065-BZXC from Cypress Semi because it has UVC drivers support. The CYUSB3065-BZXC supports only MIPI CSI-2 V1.01 whereas the DS90UB954 chip support MIPI-CSI 2 V1.3.
Is the MIPI CSI 1.3 backward compatible with MIPI CSI-2 V1.01 ? Do I have to do any special configuration for this on the Serializer and De-serializer chips? Would I face any issues?
Tony