Part Number: DSLVDS1001
Hello,
We are having a Serdes interface which requires a reference differential clock 101MHz with maximum jitter +/-10ps (Peak to Peak Jitter) . The single ended clock source with low jitter/phase noise spec is identified, however to convert it into an differential out we are considering the DSLVDS1001. So i would like to know if this device is suitable for such an application, and if so is there any additive phase noise or some jitter increase may occur which may violate the serdes chip spec.
Any suggestion will be helpful.
Thanks
Stephen