Part Number: TPS65987D
Dear TI,
I read doc slvubh2b, how to simulate to check condition of chip such as



thanks,
Tuyen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987D
Dear TI,
I read doc slvubh2b, how to simulate to check condition of chip such as



thanks,
Tuyen
Hello Tuyen,
There are two ways you can read the registers of the TPS65987D controller.
1) If you have an EVM, you could use the GUI to read the registers you desire. In the GUI, you should first setup the project for the respective PD controller. Then enable debug mode. In debug mode, you will have options to read all the registers.
2) If you are not using an EVM, then you would connect to the I2C master lines (please refer datasheet).
In this case, you should first check the mode of the PD controller. You can do this using register 0x3 (1.3.2 Unique Address Interface Registers from technical reference manual). Must ensure the PD controller is in APP mode.
Example: write to 0x20 ack data: 0x03
read to 0x20 ack data: 0x04 0x41 0x50 0x50 0x20 (Asci for APP)
The first byte represents the number of bytes sent by the PD controller. The next four bytes is ASCI for APP.
Next, write the register you like to read to the PD controller.
Example: Reading the version register.
write to 0x20 ack data: 0x0F
read to 0x20 ack data: 0x04 0x44 0x12 0x07 0xF8
The first byte represents the number of bytes sent by the PD controller. The next four byte represent data.
Result: 0xF8071244
You can perform this to any register to read their contents.
- Deepak
Thanks Deepak ,
I can read all register from MCU, my question is how to generate condition such as: Low current, Over current....to verify it? My case is need to detect low current supply to PD chip and show warning to user.
thanks,
Tuyen
Tuyen,
The way to generate low current / over current is by using an electronic loads.
- Deepak
Can you help confirm this chip can detect low current? I read all document but it seem not show register for this?
thanks,
Tuyen
Hi Tuyen,
There is no register that will give you a feedback for low current. The PD controller itself required minimal power to be on operation. The current consumed by the sink depends on the load.
- Deepak
Thanks Deepak ,
I have one question is this chip can detect USB 2.0 or 3.0 plugin? I tried plug my SINK board to USB 2.0 and 3.0 and dump all register are the same
[2022-03-31 14:09:08.210] root@SiriusI:~# , ./readI2C_PD [2022-03-31 14:09:11.756] Read all register of PD IC! [2022-03-31 14:09:11.769] Register 0x00: 28 00 00 00 [2022-03-31 14:09:11.779] Register 0x01: 41 43 45 4c [2022-03-31 14:09:11.792] Register 0x02: 01 00 00 00 [2022-03-31 14:09:11.804] Register 0x03: 41 50 50 20 [2022-03-31 14:09:11.815] Register 0x04: 00 00 00 00 [2022-03-31 14:09:11.830] Register 0x05: 0c 22 7e 02 73 d2 3b ad db 41 f0 55 c1 13 05 4c [2022-03-31 14:09:11.846] Register 0x06: 08 02 00 00 00 00 00 00 [2022-03-31 14:09:11.855] Register 0x08: 00 00 00 00 [2022-03-31 14:09:11.876] Register 0x09: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:11.885] Register 0x0f: 09 10 07 f7 [2022-03-31 14:09:11.897] Register 0x10: 00 00 00 00 [2022-03-31 14:09:11.916] Register 0x11: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:11.929] Register 0x14: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:11.942] Register 0x15: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:11.955] Register 0x16: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:09:11.967] Register 0x17: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:09:11.983] Register 0x18: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:11.995] Register 0x19: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:12.008] Register 0x1a: 1d 00 90 01 00 00 00 00 [2022-03-31 14:09:12.017] Register 0x20: 00 [2022-03-31 14:09:12.035] Register 0x21: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.047] Register 0x26: c0 00 00 00 80 00 00 00 [2022-03-31 14:09:12.059] Register 0x27: 01 00 02 00 00 00 80 00 14 14 00 00 00 78 [2022-03-31 14:09:12.075] Register 0x28: 08 58 b6 df 01 00 00 00 [2022-03-31 14:09:12.087] Register 0x29: 02 04 11 40 [2022-03-31 14:09:12.099] Register 0x2d: 1c 00 00 00 a2 06 00 00 30 00 00 00 [2022-03-31 14:09:12.117] Register 0x2e: 36 37 35 38 31 30 30 62 38 39 32 38 38 66 36 66 34 37 63 61 33 35 66 62 61 33 36 35 38 30 34 61 34 61 66 62 64 34 36 65 5f 30 31 31 32 32 30 31 38 [2022-03-31 14:09:12.134] Register 0x2f: 54 50 53 36 35 39 38 38 20 48 57 30 30 33 30 20 46 57 46 37 30 37 2e 31 30 2e 30 30 20 5a 41 63 65 31 00 00 00 00 00 41 43 45 32 00 10 07 f7 [2022-03-31 14:09:12.152] Register 0x30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.166] Register 0x31: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.186] Register 0x32: 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.207] Register 0x33: 02 5a 90 01 36 5a 90 01 99 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 2c 69 01 40 2c 69 01 40 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.213] Register 0x34: 00 00 00 00 00 00 [2022-03-31 14:09:12.230] Register 0x35: 00 00 00 00 [2022-03-31 14:09:12.240] Register 0x36: 00 00 00 00 [2022-03-31 14:09:12.252] Register 0x37: 6f 3d 3d 00 00 00 00 00 c8 90 01 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.265] Register 0x38: 01 ff 01 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.279] Register 0x3f: 33 00 [2022-03-31 14:09:12.291] Register 0x40: 14 00 05 00 [2022-03-31 14:09:12.302] Register 0x41: 00 00 00 00 [2022-03-31 14:09:12.313] Register 0x42: 1a 04 00 00 [2022-03-31 14:09:12.325] Register 0x43: 19 19 19 19 19 19 32 00 00 [2022-03-31 14:09:12.345] Register 0x47: 03 51 04 40 c4 00 00 00 00 10 07 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 10 07 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.360] Register 0x48: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.373] Register 0x49: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.393] Register 0x4a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.410] Register 0x4e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.424] Register 0x4f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.436] Register 0x50: 00 00 00 00 00 00 [2022-03-31 14:09:12.446] Register 0x51: 03 45 1c 0c 11 00 [2022-03-31 14:09:12.459] Register 0x52: 00 05 00 00 00 00 00 [2022-03-31 14:09:12.475] Register 0x57: 00 00 [2022-03-31 14:09:12.491] Register 0x58: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.502] Register 0x59: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.524] Register 0x5c: 07 80 00 00 00 00 00 00 00 80 00 00 00 00 00 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 29 03 27 00 00 00 00 00 00 00 00 00 00 00 00 2d 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 [2022-03-31 14:09:12.535] Register 0x5d: 00 00 00 00 [2022-03-31 14:09:12.545] Register 0x5f: b3 00 00 00 00 [2022-03-31 14:09:12.559] Register 0x60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.575] Register 0x61: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.587] Register 0x62: 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.601] Register 0x64: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.613] Register 0x69: 02 00 03 61 [2022-03-31 14:09:12.625] Register 0x6b: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.643] Register 0x6c: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.655] Register 0x70: 00 [2022-03-31 14:09:12.669] Register 0x71: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.684] Register 0x72: 06 80 00 00 07 80 00 00 [2022-03-31 14:09:12.697] Register 0x73: 51 04 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.709] Register 0x74: 00 00 00 00 [2022-03-31 14:09:12.720] Register 0x75: 00 00 00 00 [2022-03-31 14:09:12.735] Register 0x76: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.749] Register 0x77: 51 04 34 12 00 00 00 00 01 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.764] Register 0x78: 00 00 00 00 00 00 00 [2022-03-31 14:09:12.778] Register 0x79: 00 00 00 00 00 00 00 [2022-03-31 14:09:12.791] Register 0x7a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.806] Register 0x7b: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.818] Register 0x7c: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.837] Register 0x7d: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.852] Register 0x7e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.867] Register 0x7f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:12.869] root@SiriusI:~# [2022-03-31 14:09:15.916] root@SiriusI:~# [2022-03-31 14:09:16.089] root@SiriusI:~# [2022-03-31 14:09:16.272] root@SiriusI:~# [2022-03-31 14:09:16.441] root@SiriusI:~# [2022-03-31 14:09:16.606] root@SiriusI:~# [2022-03-31 14:09:16.779] root@SiriusI:~# lan 2 [2022-03-31 14:09:18.100] -sh: lan: command not found [2022-03-31 14:09:18.100] root@SiriusI:~# [2022-03-31 14:09:18.417] root@SiriusI:~# [2022-03-31 14:09:18.590] root@SiriusI:~# [2022-03-31 14:09:18.758] root@SiriusI:~# [2022-03-31 14:09:18.923] root@SiriusI:~# [2022-03-31 14:09:19.076] root@SiriusI:~# lan 2./readI2C_PD [2022-03-31 14:09:20.550] Read all register of PD IC! [2022-03-31 14:09:20.561] Register 0x00: 28 00 00 00 [2022-03-31 14:09:20.574] Register 0x01: 41 43 45 4c [2022-03-31 14:09:20.585] Register 0x02: 01 00 00 00 [2022-03-31 14:09:20.597] Register 0x03: 41 50 50 20 [2022-03-31 14:09:20.609] Register 0x04: 00 00 00 00 [2022-03-31 14:09:20.624] Register 0x05: 0c 22 7e 02 73 d2 3b ad db 41 f0 55 c1 13 05 4c [2022-03-31 14:09:20.637] Register 0x06: 08 02 00 00 00 00 00 00 [2022-03-31 14:09:20.646] Register 0x08: 00 00 00 00 [2022-03-31 14:09:20.665] Register 0x09: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:20.678] Register 0x0f: 09 10 07 f7 [2022-03-31 14:09:20.692] Register 0x10: 00 00 00 00 [2022-03-31 14:09:20.713] Register 0x11: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:20.724] Register 0x14: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:20.736] Register 0x15: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:20.748] Register 0x16: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:09:20.760] Register 0x17: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:09:20.773] Register 0x18: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:20.786] Register 0x19: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:09:20.802] Register 0x1a: 1d 00 90 01 00 00 00 00 [2022-03-31 14:09:20.812] Register 0x20: 00 [2022-03-31 14:09:20.828] Register 0x21: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:20.843] Register 0x26: c0 00 00 00 80 00 00 00 [2022-03-31 14:09:20.853] Register 0x27: 01 00 02 00 00 00 80 00 14 14 00 00 00 78 [2022-03-31 14:09:20.867] Register 0x28: 08 58 b6 df 01 00 00 00 [2022-03-31 14:09:20.876] Register 0x29: 02 04 11 40 [2022-03-31 14:09:20.893] Register 0x2d: 1c 00 00 00 a2 06 00 00 30 00 00 00 [2022-03-31 14:09:20.914] Register 0x2e: 36 37 35 38 31 30 30 62 38 39 32 38 38 66 36 66 34 37 63 61 33 35 66 62 61 33 36 35 38 30 34 61 34 61 66 62 64 34 36 65 5f 30 31 31 32 32 30 31 38 [2022-03-31 14:09:20.930] Register 0x2f: 54 50 53 36 35 39 38 38 20 48 57 30 30 33 30 20 46 57 46 37 30 37 2e 31 30 2e 30 30 20 5a 41 63 65 31 00 00 00 00 00 41 43 45 32 00 10 07 f7 [2022-03-31 14:09:20.944] Register 0x30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:20.956] Register 0x31: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:20.976] Register 0x32: 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:20.995] Register 0x33: 02 5a 90 01 36 5a 90 01 99 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 2c 69 01 40 2c 69 01 40 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.007] Register 0x34: 00 00 00 00 00 00 [2022-03-31 14:09:21.018] Register 0x35: 00 00 00 00 [2022-03-31 14:09:21.030] Register 0x36: 00 00 00 00 [2022-03-31 14:09:21.044] Register 0x37: 6f 3d 3d 00 00 00 00 00 c8 90 01 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.058] Register 0x38: 01 ff 01 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.069] Register 0x3f: 33 00 [2022-03-31 14:09:21.081] Register 0x40: 14 00 05 00 [2022-03-31 14:09:21.094] Register 0x41: 00 00 00 00 [2022-03-31 14:09:21.105] Register 0x42: 1a 04 00 00 [2022-03-31 14:09:21.117] Register 0x43: 19 19 19 19 19 19 32 00 00 [2022-03-31 14:09:21.135] Register 0x47: 03 51 04 40 c4 00 00 00 00 10 07 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 10 07 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.150] Register 0x48: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.165] Register 0x49: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.186] Register 0x4a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.203] Register 0x4e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.218] Register 0x4f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.230] Register 0x50: 00 00 00 00 00 00 [2022-03-31 14:09:21.243] Register 0x51: 03 45 1c 0c 11 00 [2022-03-31 14:09:21.254] Register 0x52: 00 05 00 00 00 00 00 [2022-03-31 14:09:21.264] Register 0x57: 00 00 [2022-03-31 14:09:21.280] Register 0x58: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.293] Register 0x59: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.315] Register 0x5c: 07 80 00 00 00 00 00 00 00 80 00 00 00 00 00 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 29 03 27 00 00 00 00 00 00 00 00 00 00 00 00 2d 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 [2022-03-31 14:09:21.327] Register 0x5d: 00 00 00 00 [2022-03-31 14:09:21.339] Register 0x5f: b3 00 00 00 00 [2022-03-31 14:09:21.354] Register 0x60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.368] Register 0x61: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.380] Register 0x62: 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.394] Register 0x64: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.406] Register 0x69: 02 00 03 61 [2022-03-31 14:09:21.417] Register 0x6b: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.436] Register 0x6c: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.451] Register 0x70: 00 [2022-03-31 14:09:21.465] Register 0x71: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.477] Register 0x72: 06 80 00 00 07 80 00 00 [2022-03-31 14:09:21.492] Register 0x73: 51 04 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.503] Register 0x74: 00 00 00 00 [2022-03-31 14:09:21.514] Register 0x75: 00 00 00 00 [2022-03-31 14:09:21.528] Register 0x76: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.543] Register 0x77: 51 04 34 12 00 00 00 00 01 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.557] Register 0x78: 00 00 00 00 00 00 00 [2022-03-31 14:09:21.565] Register 0x79: 00 00 00 00 00 00 00 [2022-03-31 14:09:21.585] Register 0x7a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.600] Register 0x7b: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.611] Register 0x7c: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.630] Register 0x7d: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.648] Register 0x7e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.663] Register 0x7f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:09:21.673] root@SiriusI:~#
[2022-03-31 14:32:57.593] root@SiriusI:~# ./readI2C_PD [2022-03-31 14:33:06.230] Read all register of PD IC! [2022-03-31 14:33:06.243] Register 0x00: 28 00 00 00 [2022-03-31 14:33:06.254] Register 0x01: 41 43 45 4c [2022-03-31 14:33:06.265] Register 0x02: 01 00 00 00 [2022-03-31 14:33:06.276] Register 0x03: 41 50 50 20 [2022-03-31 14:33:06.289] Register 0x04: 00 00 00 00 [2022-03-31 14:33:06.302] Register 0x05: 0c 22 7e 02 73 d2 3b ad db 41 f0 55 c1 13 05 4c [2022-03-31 14:33:06.314] Register 0x06: 08 02 00 00 00 00 00 00 [2022-03-31 14:33:06.327] Register 0x08: 00 00 00 00 [2022-03-31 14:33:06.346] Register 0x09: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.357] Register 0x0f: 09 10 07 f7 [2022-03-31 14:33:06.370] Register 0x10: 00 00 00 00 [2022-03-31 14:33:06.392] Register 0x11: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.405] Register 0x14: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:33:06.417] Register 0x15: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:33:06.430] Register 0x16: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:33:06.444] Register 0x17: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:33:06.455] Register 0x18: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:33:06.468] Register 0x19: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:33:06.480] Register 0x1a: 1d 00 90 01 00 00 00 00 [2022-03-31 14:33:06.492] Register 0x20: 00 [2022-03-31 14:33:06.510] Register 0x21: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.522] Register 0x26: c0 00 00 00 80 00 00 00 [2022-03-31 14:33:06.536] Register 0x27: 01 00 02 00 00 00 80 00 14 14 00 00 00 78 [2022-03-31 14:33:06.548] Register 0x28: 08 58 b6 df 01 00 00 00 [2022-03-31 14:33:06.559] Register 0x29: 02 04 11 40 [2022-03-31 14:33:06.573] Register 0x2d: 1c 00 00 00 a2 06 00 00 30 00 00 00 [2022-03-31 14:33:06.592] Register 0x2e: 36 37 35 38 31 30 30 62 38 39 32 38 38 66 36 66 34 37 63 61 33 35 66 62 61 33 36 35 38 30 34 61 34 61 66 62 64 34 36 65 5f 30 31 31 32 32 30 31 38 [2022-03-31 14:33:06.609] Register 0x2f: 54 50 53 36 35 39 38 38 20 48 57 30 30 33 30 20 46 57 46 37 30 37 2e 31 30 2e 30 30 20 5a 41 63 65 31 00 00 00 00 00 41 43 45 32 00 10 07 f7 [2022-03-31 14:33:06.624] Register 0x30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.639] Register 0x31: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.658] Register 0x32: 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.677] Register 0x33: 02 5a 90 01 36 5a 90 01 99 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 2c 69 01 40 2c 69 01 40 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.689] Register 0x34: 00 00 00 00 00 00 [2022-03-31 14:33:06.700] Register 0x35: 00 00 00 00 [2022-03-31 14:33:06.711] Register 0x36: 00 00 00 00 [2022-03-31 14:33:06.727] Register 0x37: 6f 3d 3d 00 00 00 00 00 c8 90 01 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.740] Register 0x38: 01 ff 01 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.751] Register 0x3f: 33 00 [2022-03-31 14:33:06.763] Register 0x40: 14 00 05 00 [2022-03-31 14:33:06.774] Register 0x41: 00 00 00 00 [2022-03-31 14:33:06.788] Register 0x42: 1a 04 00 00 [2022-03-31 14:33:06.798] Register 0x43: 19 19 19 19 19 19 32 00 00 [2022-03-31 14:33:06.817] Register 0x47: 03 51 04 40 c4 00 00 00 00 10 07 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 10 07 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.832] Register 0x48: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.848] Register 0x49: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.867] Register 0x4a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.883] Register 0x4e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.897] Register 0x4f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.909] Register 0x50: 00 00 00 00 00 00 [2022-03-31 14:33:06.919] Register 0x51: 03 45 1c 0c 11 00 [2022-03-31 14:33:06.932] Register 0x52: 00 05 00 00 00 00 00 [2022-03-31 14:33:06.944] Register 0x57: 00 00 [2022-03-31 14:33:06.960] Register 0x58: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.975] Register 0x59: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:06.995] Register 0x5c: 07 80 00 00 00 00 00 00 00 80 00 00 00 00 00 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 29 03 27 00 00 00 00 00 00 00 00 00 00 00 00 2d 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 [2022-03-31 14:33:07.006] Register 0x5d: 00 00 00 00 [2022-03-31 14:33:07.018] Register 0x5f: b3 00 00 00 00 [2022-03-31 14:33:07.034] Register 0x60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.049] Register 0x61: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.061] Register 0x62: 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.075] Register 0x64: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.087] Register 0x69: 02 00 03 61 [2022-03-31 14:33:07.099] Register 0x6b: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.119] Register 0x6c: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.130] Register 0x70: 00 [2022-03-31 14:33:07.145] Register 0x71: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.156] Register 0x72: 06 80 00 00 07 80 00 00 [2022-03-31 14:33:07.170] Register 0x73: 51 04 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.182] Register 0x74: 00 00 00 00 [2022-03-31 14:33:07.194] Register 0x75: 00 00 00 00 [2022-03-31 14:33:07.208] Register 0x76: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.223] Register 0x77: 51 04 34 12 00 00 00 00 01 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.238] Register 0x78: 00 00 00 00 00 00 00 [2022-03-31 14:33:07.250] Register 0x79: 00 00 00 00 00 00 00 [2022-03-31 14:33:07.266] Register 0x7a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.280] Register 0x7b: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.293] Register 0x7c: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.313] Register 0x7d: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.328] Register 0x7e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.342] Register 0x7f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:33:07.350] root@SiriusI:~# [2022-03-31 14:33:07.978] root@SiriusI:~# [2022-03-31 14:33:08.189] root@SiriusI:~# [2022-03-31 14:33:08.394] root@SiriusI:~# [2022-03-31 14:33:08.594] root@SiriusI:~# [2022-03-31 14:33:08.802] root@SiriusI:~# [2022-03-31 14:33:09.026] root@SiriusI:~# [2022-03-31 14:33:09.221] root@SiriusI:~# [2022-03-31 14:33:09.447] root@SiriusI:~# [2022-03-31 14:33:09.641] root@SiriusI:~# [2022-03-31 14:37:13.601] root@SiriusI:~# [2022-03-31 14:37:13.785] root@SiriusI:~# [2022-03-31 14:37:13.958] root@SiriusI:~# [2022-03-31 14:37:22.647] root@SiriusI:~# [2022-03-31 14:37:22.866] root@SiriusI:~# ./readI2C_PD [2022-03-31 14:37:30.076] Read all register of PD IC! [2022-03-31 14:37:30.088] Register 0x00: 28 00 00 00 [2022-03-31 14:37:30.101] Register 0x01: 41 43 45 4c [2022-03-31 14:37:30.113] Register 0x02: 01 00 00 00 [2022-03-31 14:37:30.123] Register 0x03: 41 50 50 20 [2022-03-31 14:37:30.136] Register 0x04: 00 00 00 00 [2022-03-31 14:37:30.149] Register 0x05: 0c 22 7e 02 73 d2 3b ad db 41 f0 55 c1 13 05 4c [2022-03-31 14:37:30.161] Register 0x06: 08 02 00 00 00 00 00 00 [2022-03-31 14:37:30.173] Register 0x08: 00 00 00 00 [2022-03-31 14:37:30.194] Register 0x09: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.205] Register 0x0f: 09 10 07 f7 [2022-03-31 14:37:30.218] Register 0x10: 00 00 00 00 [2022-03-31 14:37:30.238] Register 0x11: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.248] Register 0x14: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:37:30.262] Register 0x15: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:37:30.275] Register 0x16: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:37:30.287] Register 0x17: 08 00 00 02 00 00 00 00 00 00 03 [2022-03-31 14:37:30.303] Register 0x18: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:37:30.315] Register 0x19: 08 00 00 02 00 00 00 00 00 00 01 [2022-03-31 14:37:30.327] Register 0x1a: 1d 00 90 01 00 00 00 00 [2022-03-31 14:37:30.339] Register 0x20: 00 [2022-03-31 14:37:30.356] Register 0x21: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.369] Register 0x26: c0 00 00 00 80 00 00 00 [2022-03-31 14:37:30.382] Register 0x27: 01 00 02 00 00 00 80 00 14 14 00 00 00 78 [2022-03-31 14:37:30.394] Register 0x28: 08 58 b6 df 01 00 00 00 [2022-03-31 14:37:30.406] Register 0x29: 02 04 11 40 [2022-03-31 14:37:30.419] Register 0x2d: 1c 00 00 00 a2 06 00 00 30 00 00 00 [2022-03-31 14:37:30.437] Register 0x2e: 36 37 35 38 31 30 30 62 38 39 32 38 38 66 36 66 34 37 63 61 33 35 66 62 61 33 36 35 38 30 34 61 34 61 66 62 64 34 36 65 5f 30 31 31 32 32 30 31 38 [2022-03-31 14:37:30.455] Register 0x2f: 54 50 53 36 35 39 38 38 20 48 57 30 30 33 30 20 46 57 46 37 30 37 2e 31 30 2e 30 30 20 5a 41 63 65 31 00 00 00 00 00 41 43 45 32 00 10 07 f7 [2022-03-31 14:37:30.469] Register 0x30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.485] Register 0x31: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.505] Register 0x32: 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 90 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.523] Register 0x33: 02 5a 90 01 36 5a 90 01 99 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 2c 69 01 40 2c 69 01 40 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.536] Register 0x34: 00 00 00 00 00 00 [2022-03-31 14:37:30.547] Register 0x35: 00 00 00 00 [2022-03-31 14:37:30.559] Register 0x36: 00 00 00 00 [2022-03-31 14:37:30.575] Register 0x37: 6f 3d 3d 00 00 00 00 00 c8 90 01 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.586] Register 0x38: 01 ff 01 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.598] Register 0x3f: 33 00 [2022-03-31 14:37:30.610] Register 0x40: 14 00 05 00 [2022-03-31 14:37:30.621] Register 0x41: 00 00 00 00 [2022-03-31 14:37:30.633] Register 0x42: 1a 04 00 00 [2022-03-31 14:37:30.646] Register 0x43: 19 19 19 19 19 19 32 00 00 [2022-03-31 14:37:30.664] Register 0x47: 03 51 04 40 c4 00 00 00 00 10 07 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 10 07 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.679] Register 0x48: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.694] Register 0x49: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.714] Register 0x4a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.730] Register 0x4e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.745] Register 0x4f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.756] Register 0x50: 00 00 00 00 00 00 [2022-03-31 14:37:30.769] Register 0x51: 03 45 1c 0c 11 00 [2022-03-31 14:37:30.781] Register 0x52: 00 05 00 00 00 00 00 [2022-03-31 14:37:30.792] Register 0x57: 00 00 [2022-03-31 14:37:30.809] Register 0x58: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.823] Register 0x59: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.841] Register 0x5c: 07 80 00 00 00 00 00 00 00 80 00 00 00 00 00 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 29 03 27 00 00 00 00 00 00 00 00 00 00 00 00 2d 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 [2022-03-31 14:37:30.853] Register 0x5d: 00 00 00 00 [2022-03-31 14:37:30.864] Register 0x5f: b3 00 00 00 00 [2022-03-31 14:37:30.880] Register 0x60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.895] Register 0x61: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.908] Register 0x62: 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.921] Register 0x64: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.933] Register 0x69: 02 00 03 61 [2022-03-31 14:37:30.946] Register 0x6b: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.965] Register 0x6c: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:30.976] Register 0x70: 00 [2022-03-31 14:37:30.992] Register 0x71: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.004] Register 0x72: 06 80 00 00 07 80 00 00 [2022-03-31 14:37:31.019] Register 0x73: 51 04 34 12 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.030] Register 0x74: 00 00 00 00 [2022-03-31 14:37:31.042] Register 0x75: 00 00 00 00 [2022-03-31 14:37:31.057] Register 0x76: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.071] Register 0x77: 51 04 34 12 00 00 00 00 01 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.084] Register 0x78: 00 00 00 00 00 00 00 [2022-03-31 14:37:31.096] Register 0x79: 00 00 00 00 00 00 00 [2022-03-31 14:37:31.110] Register 0x7a: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.126] Register 0x7b: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.139] Register 0x7c: 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.158] Register 0x7d: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.172] Register 0x7e: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.187] Register 0x7f: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [2022-03-31 14:37:31.189] root@SiriusI:~#
Tuyen
Tuyen,
Currently there is no register or support to detect of the far end connected is a usb2.0 or usb3.0. I also did a comparison of the logs and recheck and found the same.
However, you can use the status register (bit 24:25), to check if the far end is acting as legacy. (if you would like to know if the far end is typeC or typeA.
- Deepak
-