Part Number: SN65DPHY440SS
Hi Team,
My customer is using SN65DPHY440SS for their project evaluation. One scenario from datasheet is described following:

- Customer is using 1.5Gbps, and they would like to know the input trace for 12 inch is the maximum value or a typical value for this case? If this is the typical value, what is the maximum value for this case?
- For the trace between SN65dphy440ss and APU is 1inch, is it a maximum value or typical value for 1.5Gbps? Can SN65DPHY440SS accept more than 1inch if the APU can accept the length in approximate 4inch?
- If the camera is 35cm length from APU, at which position is recommended to put the SN65DPHY440SS? Close to Camera or APU?
Thank you for the support, and I look forward to hearing from you.