Other Parts Discussed in Thread: TUSB8042A, TUSB3410, TUSB320
Hello!
Iam searching for an USB 3.2 hub IC solution that is very easy to implement and needs no additional programming. The hub should offer at least four standard downstream ports for USB devices and provide minimum 0.9A@5V continuously for every port. I looked at the TUSB8042A as a possible soultion but I am not sure if this is the correct one.
The four devices that will be attached to the hub are serial communicating devices (UART or RS232). They would also need protocol shifting ICs like FTDI chips to shift their serial protocol to USB 3.2 protocol and act as a normal COM port (CDC).
I am looking forward to some useful suggestions. Thanks!