This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1791: Protection on Y and Z Lines

Part Number: SN65HVD1791


Hi,

Good day. I hope you are doing well.

On the SN65HVD1791D, table 7.1 indicates that the A and B lines are protected against over-Voltage, are the Y and Z lines also protected?

Thank you.


Regards,

Cedrick

  • Hi Cedrick,

    I am checking with our internal team as this is a bit of an older device to get confirmation on all of our specs. I should have something to you within the next 24 hours - I do think the Y/Z pins are protected; however, the datasheet is confusing and seemingly contradicts itself so I want to double check. Stay posted I should have information very soon to confirm this spec.

    Best,

    Parker Dodson

  • Hi Cedrick,

    The Y/Z pins on the 91 should be protected up to +/-70V. The datasheet didn't specify the Y/Z pins except on the devices that are lower than +/-30V - but the datasheet indicates that the 91 will have its RS-485 bus pins protected to +/-70V, which Y,Z,A, and B are the bus pins.

    Best,

    Parker Dodson