Part Number: ONET1151L
I have a design that was based on the reference schematic that is on your website.

In this case the PD pin is tied to the CATHODE of the PD in the TOSA. I see in the datasheet that the photo diode is connected in this way....

I also see that I can change the direction of current flow from the PD pin on the ONET1151L by setting register values. In my case, the TOSA that I have has the ANODE of the photo diode connected to a pin. The CATHODE of the photo diode is connected to the ANODE of the laser. So my configuration would look like the following...

My question is, assuming that I flip the direction of the PD pin on the ONET1151L, will the circuit function correctly with my specific TOSA with the connections shown above?